Skip to main content
Engineer adjusts a component in a test fixture with a CAD model displayed on a nearby computer screen.

High-Reliability Connectors for Automotive Connectivity

A significant share of automotive technical risk lies in inconsistent reliability across electrical connections. As vehicle architectures evolve with electrification, autonomous driving and high-speed data networks, the demands on connectors have fundamentally changed. Engineers need assurance that subsystem components will not just pass validation, but can perform reliably under real-world conditions over the full vehicle lifetime.

Through its Design for Reliability (DfR) methodology, Molex embeds reliability into the product development cycle from the earliest design phases, applying physics-of-failure analysis, accelerated life testing and failure mode identification well before validation begins. This proactive approach helps reduce late-cycle failures, costly design changes and requalification loops.

Reliability Testing and Validation in Automotive Connectors


Validation gaps found under test conditions such as vibration, thermal cycling and mechanical stress are often traced to standard connectors that lack application-specific design, leading to field failures and warranty returns. Within OEM design workflows, non-compliant connectors can also cause program delays due to insufficient validation data.

Engineering teams need a consistent, physics-based validation framework that ensures quality materials, tolerances and performance benchmarks are aligned with standards that govern automotive connectors: USCAR2, GMW3191, LV214, IEC 60512 and ISO 16750.

Molex invests in dedicated DfR engineering resources because meeting a specification is not the same as understanding true field reliability. Where standard validation confirms a pass/fail, DfR identifies where  a connector may eventually fail. By uncovering design margins anddegradation mechanisms that compliance tests may miss, OEM engineers benefit from a qualified part and a clear roadmap for its performance over the vehicle’s lifetime.

Maintaining Consistent Quality Across Global Manufacturing


Using Test-to-Failure to Validate Long-Term Automotive Performance

Traditional testing strategies estimate the impact of field conditions on components, but these forecasts do not capture all vulnerabilities of newer automotive architectures. Test-to-failure methodology provides deeper insight by straining parts to the point of mechanical or thermal breakdown, then using the data to train predictive AI and machine-learning models.

Find out how Molex uses digital twins and data insights to align the strength and lifespan of high-performance connectors to regulatory demands.

An engineer inspects a virtual model of automotive high-performance components.

Component-Level Digital Twins: Accelerating Automotive Innovation

Rising vehicle complexity is tightening space and weight constraints, while 14-week testing cycles slow progress toward production. See how Molex uses digital twins and 3D modeling to validate performance early, reducing reliance on physical prototypes and enabling more compact, reliable designs.

Engineers discuss a heat map of high-performance automotive components under testing.

Quantifying Reliability in Modern Vehicles

To quantify reliability, identify system failure modes and establish safety margins, internal validation teams need a different approach than standard go/no-go testing. To move beyond simple pass/fail metrics, automakers are adopting stress-life modeling, a more comprehensive method of examining lifecycle physics.

Find out how Molex uses predictive models to inform its manufacturing process, from cost estimates to material selection, for faster time to market.

A stylized schematic of electrical architecture in a modern vehicle.

Capability

The Global Reliability Lab

At the Molex Global Reliability Lab, the quality and long-term reliability of new product designs are refined and tested, giving customers access to decades of engineering expertise and knowledge of manufacturing best practices. This high-tech facility aids engineering teams from the start of product development and consults on challenges as they emerge, reducing the risk of unwanted surprises and rework. Find out how Molex engineering collaboration can benefit your project.

An electromagnetic field receiver for measurement.

ON-DEMAND WEBINAR

Crimp Performance Unveiled: The Crucial Role of Wire Quality

Testing wire quality and crimp integrity reveals significant reliability risks in automotive environments. Well-defined terminations and improved installation procedures reduce wire variability and help maintain long-term stability.

This on-demand webinar shows how to prevent harness failure and maximize crimped connector performance.

A presentation slide from an on-demand webinar on crimp performance in automotive reliability testing.