Skip to main content

Leak Detection Cables

A customizable solution for server applications, Molex Leak Detection Cables provide flexible, high-reliability monitoring for early leak detection in liquid-cooled data center environments. Designed for space-constrained server trays, these assemblies integrate seamlessly with Molex connectors and monitoring systems to safeguard uptime and protect key infrastructure.

Voltage Circuits
Up to 300V Custom

Features and Benefits


As data centers adopt liquid cooling to support high-density computing, AI workloads and energy efficiency, the risk of fluid leaks becomes a pressing concern. Static interconnect solutions force costly overhauls to meet future bandwidth and power demands. A lack of modularity and backward compatibility slows innovation and increases the total cost of ownership. As power densities rise, connectors and cables that cannot withstand elevated temperatures become points of failure, leading to unplanned downtime, increased maintenance and premature equipment replacement—especially in thermally stressed, liquid-cooled environments.

Manufacturers need scalable solutions that detect leaks, preventing significant damage within data center rack trays. Additionally, small wire diameters for space-constrained applications are necessary. To avoid costly downtime, equipment failure and data loss, a proactive alert system is crucial.

Molex Leak Detection Cables provide an essential safeguard in modern data centers that use liquid cooling systems instead of traditional air-based cooling to improve efficiency and thermal performance. These compact cable assemblies feature small wire diameters, helping prevent damage to server racks and trays by identifying fluid intrusion before it escalates. Data center operators can maintain uptime, protect high-value assets and align with the industry shift toward intelligent, resilient infrastructure. With seamless integration, Leak Detection Cables enable easy implementation without major system overhauls.

Scalable Configurations and Customizable

Leak Detection Cables integrate seamlessly with Molex connectors and monitoring systems to facilitate scalable architecture that supports a range of data center layouts and cooling strategies. This customizable solution enables data centers to stay ahead of evolving cooling technologies and avoid operational risks.

Custom leak detection cable with Micro-Lock Plus connector.

Smart Detection System for Operational Efficiency

These cable assemblies are a part of a smart detection system, alerting operators to leaks before they escalate into costly failures or downtime. By providing an early warning and enabling a rapid response, manufacturers can protect high-value equipment, maintain uptime and avoid expensive repairs.

Rope style leak detection cable for early warning alerts.

Engineered for Space-Constrained Environments

For tight server configurations, these Leak Detection Cables have a compact design with small wire diameters to maximize available space and support high-density configurations.

Small leak detection cable with Micro-Lock Plus connector.

Saves cost and time by avoiding expensive repairs and delayed operations
Liquid-detection capabilities enable early leak detection before any damage occurs within the server rack.

Resists abrasion, contamination and false alarms
These cable assemblies are designed for durability even in high-humidity or dust-prone environments that can cause equipment failure.

Optimizes space to overcome footprint limitations
With a small wire diameter and form factor, these cables offer an exceptional solution for space-constrained applications that utilize connectors with small housing dimensions such as Micro-Lock Plus and Micro-Fit Connectors.

Provides a total solution for all elements required, mitigating integration complexities
Multiple connector options, leak cables and monitor cables are part of the complete solution.

Enables design flexibility to overcome configuration limitations
These cable assemblies are customizable and facilitate easy modifications, reducing time delays.

Datasheets and Guides


Applications by Industry


Liquid-cooled server racks

This is not a definitive list of applications for this product. It represents some of the more common uses.

Frequently Asked Questions


What are Leak Detection Cables?

Leak Detection Cables are a customizable leak-monitoring solution that is used predominantly in data center rack trays and server applications where early detection of liquid intrusion can prevent equipment damage, downtime, safety risks and costly cleanup.

How do Leak Detection Cables work?

Leak detection cables work on the principle that moisture creates an electrical bridge between two conductors, triggering an alert before equipment is damaged. In normal situations, the conductors are kept electrically isolated.

Rope-style leak detection cables use a braided, flexible outer structure that keeps the conductors separated while still allowing moisture to reach them. When water contacts the cable, the liquid forms a conductive path, creating a short that is sent to the monitor to notify the operator.

Discrete wire leak detection cables connect the monitoring system to the flexible printed circuit (FPC). The FPC has parallel conducting printed circuits that do not touch each other, and the FPC is laid out on critical areas of the tray. When the conductors come in contact with water, the liquid bridges the conductors, creating a short that is sent to the monitor to notify the operator. The cable assemblies incorporate small connectors such as Micro-Lock Plus, Micro-Fit or Nano-Fit Connectors to provide a solution. The cable and FPC solution is more widely used since the FPC covers a wider area than the rope-style alternative.

Is there a sensor in the cable assemblies?

There are no sensors in the cable assemblies. Instead, two braided conductors function as a sensor in the rope-type cables. The discrete-type cables use FPCs to provide parallel circuits.

How do Leak Detection Cables create value for customers?

Leak Detection Cables help customers detect liquid leakage early, including water and water/glycol mixtures. Once there is a leakage signal, customers will determine the problem area early enough to help prevent process failure and system damage.