In the early stages of the COVID-19 pandemic, University Hospital Limerick (UHL) in Ireland knew there would likely be a spike in the demand for respiratory technologies. In an effort to get ahead of the potential need, UHL reached out to the Rapid Innovation Unit (RIU), an SFI supported research group through the CONFIRM Smart Manufacturing Center in University of Limerick (UL), for help. This set off a chain of efforts, including turning to Molex for design and sourcing expertise.
The RIU team, together with a network of associated industry partners, identified a respiratory adapter to accommodate viral filters to help protect healthcare staff treating COVID positive and COVID suspect patients over the next 12-18 months. However, in addition to providing proper functionality, it was also important to ensure the adapter could be mass produced in a short amount of time, and this is where Molex proved invaluable.
By implementing a design for manufacture (DFM) process and leveraging our existing knowledge of medical grade materials, Molex was able to suggest design optimizations and ultimately developed the prototype in less than two weeks.