The concept of the “software-defined vehicle” is gaining momentum throughout the automotive industry. The way in which drivers and passengers will experience the car of the future is dependent on the software and related services offered by the car manufacturer. This will impact dramatically the architecture of the car as well as the bandwidth of in-vehicle networks (IVNs), which will continue to grow exponentially, as will the complications associated with high data rates.
The automotive industry is projected to see an estimated 33.57% compound annual growth rate (CAGR)1 (2015-2035) of Level 2-5 ADAS technologies. Both current and future adaptive and automated applications will contribute to this rise with an estimated 7.89% CAGR1 (2017-2026) and will influence IVN communication designs. For example, IVN designers will face <10ms deterministic latency requirements and the need to mitigate increases in the volume of “jitter” or interfering data that can significantly affect the data delivery required per the classification or priority to support the application’s intent.