The ease-of-use consumers experience with their cellphones and laptops has created a high bar for medical device manufacturers. In fact, the Molex survey shows that 43% of design engineers said higher customer expectations are complicating design efforts. “The user experience has suddenly become much more important. If people don’t like the way a device works or find it difficult to use, they won’t use it. It’s really challenging for medical device makers,” Bedford says.
In addition, medical designers are often starting from ground zero, rather than iterating based on years of user study. Even established, widely-available devices are not always up to par. In a 2020 academic study examining consumer operation of blood pressure monitors and pulse oximeters, researchers found “a lack of usability for both devices.”
The study was conducted with healthy volunteers. But remember, outcomes could be even worse for acute patients, researchers warned: “Indeed, the patient will be in a postsurgical context, with pain, nausea, and stress, and will often need the help of family members to use the devices at home.”
Another wrinkle is the propensity to experiment with devices, which could be dangerous in a medical setting. “With a phone, you can play around with the settings to make it work. Doing that with a medical device, you may find you’ve given yourself a wrong injection,” Bedford says.
To pick up the pace of usability improvements, engineers are increasingly adopting agile development processes. In the Molex survey, more than half of design engineer teams said they have adopted agile methods, continuous innovation/continuous delivery processes, or both.
Agile development and continuous integration allow designers to make more frequent code changes, enhancing collaboration and improving designs. The process also enables regular cybersecurity reviews to avoid last-minute pressures and bug-ridden initial releases.
Having a diversified team also helps improve design. Engineers with different types of expertise can share insights, improving the overall product. The recent Molex survey indicates that in recent years, nearly half of designers have added engineers with deep expertise in specialized areas.
At Phillips-Medisize, a Molex company, engineers from diverse backgrounds have helped UX teams expand their points of view.
“We have trained and qualified user experience designers, including people who have worked in the design of consumer products and are bringing that knowledge across,” Simpson says. “Consumer products are designed to create an engaging experience. Why wouldn’t we want to see more of that in medical devices?”