Noise can come from many sources external to the cable but also from the cable or wire itself. Noise generated within a cable is often called handling noise or cable noise, but this type of unwanted signal is more accurately described as triboelectric noise.When measuring low-level signals, noise in cable or wire may be problematic. Noise in an ECG or other medical signal may make accurate diagnosis difficult or even impossible.
Recognizing that amount of triboelectric noise in medical cables should be minimized, The AAMI/ANSI EC53 requires the maximum peak-to-peak noise shall be less than 50 micro-volts (µV). Many device manufacturers specify even lower noise limits for their cables and leadwires.