As vehicles rely on increasingly complex systems and build in new functions, the number of circuits rises. To accommodate these circuits without increasing the weight or size of vehicles, miniaturization plays an outsized role. But there’s a catch.
Smaller terminals tend to have lower normal forces, especially at end-of-life, which can negatively impact electrical contact resistance. These terminals can also be subjected to repeated insertion, decoupling, and operational micro-motion (fretting). As a result, the layer of Tin on the terminal blade is worn down, exposing the underling metals to corrosive effects. This, in turn, increases electrical resistance in the circuit, compromising its performance. After multiple insertion and decoupling cycles, as the top Tin plating gradually wears away, it typically piles up at the end of the wear track on the blade. The gradual wearing down of the surface changes the physical characteristics of the interface, which can negatively impact the mate force and electrical contact resistance.
Mate force plays a key ergonomic role in the connector industry. Automotive line workers will struggle to repeatedly mate anything above 75 N. This limit puts constraints on the number of terminals that can be designed into a connector without mate assistance. Consequently, it becomes imperative to reduce the friction at each individual terminal interface to lower mate force on high-circuit count hand-mate connectors.
In general, friction and electrical contact resistance have an inverse relationship. So, the challenge is to strike the right balance and maintain both low mate force and low and stable electrical resistance over time. Consider the growing number of miniaturized electrical systems in vehicles, and it's easy to appreciate the scope of the challenge.