The rapid shift from physical buttons to touch screens and capacitive touch switches has been fueled by the widespread adoption of smartphones as well as advances in the technology and materials utilized in user interface construction. While touch screens involve a transparent surface over living LCD screens, capacitive touch switches have a predefined location of keys or sliders that are mounted behind fixed graphics. As a finger gets near it, a capacitive sensor senses the change in the electrical field around the defined area and reports to the microchip that touch has been initiated. No direct contact is needed with capacitive sensors; in fact, the strength and length of touch can be calibrated using software.
Recent advances in the sensitivity and accuracy of the sensors, as well as the film or overlays that signify the “buttons,” have made capacitive touch interfaces elegant, durable and flexible. This has opened the door to a wide variety of use cases, components and features when the right tools and materials are used. By working with an experienced supplier such as Molex, manufacturers and designers can ensure that the components of a capacitive interface—sensors, overlays, adhesives and more—are the best fit for the product.