Skip to main content
Industrial robotic arm works on electronic components along an automated manufacturing line.

Bypassing the Enclosure: The Shift to On-Machine Distributed I/O

As industrial automation scales, routing complex wiring back to central control cabinets can create commissioning bottlenecks and restrict factory floor space. Moving power, signal and data directly onto the machine frame solves these physical constraints without sacrificing network reliability in harsh industrial environments.

Read Time: 5 Min

Traditional automation systems rely on large, centralized control panels to house banks of controllers and motor drives. While these centralized enclosures remain a practical choice for smaller, contained applications, scaling them limits manufacturing layout flexibility. Designing and fabricating these custom sheet metal cabinets for large-scale operations adds high upfront cost and consumes valuable factory floor space.

As device manufacturers build intelligence directly into smaller components, engineers can leverage on-machine distributed I/O to place control directly on the equipment. Moving these components out of the cabinet greatly reduces copper cabling and creates an open floor plan that easily accommodates new workstations. Because of this localized intelligence, maintenance personnel can pinpoint exact sensor failures in real time rather than searching a massive factory floor for a single malfunctioning indicator light.

While decentralization solves spatial limitations, moving sensitive connections out of a protected enclosure forces engineers to confront the physical realities of routing cables through harsh industrial environments.

Eliminating Wiring Bottlenecks and Environmental Threats on the Machine Frame

Centralized control architectures require engineers to navigate commissioning delays caused by manual hardwiring and the physical strain placed on moving equipment. Once engineers move these connections outside the cabinet, they must also protect the network from severe environmental hazards.

Commissioning Delays and Labor Costs

System integrators typically build and test the entire automation system on their shop floor before tearing it down for shipment. Consequently, reinstalling and manually rewiring the system at the end-user plant results in substantial labor costs and increases the risk of installation errors. If mistakes occur, troubleshooting a wiring error during the final facility launch halts production and delays deployment.

Physical Strain on Moving Equipment

Beyond the initial setup, extensive cabling adds physical strain to robotic tracks and moving machine parts. Over time, continuous flexing and dragging accelerate mechanical wear on the copper conductors and can eventually lead to electrical faults.

Environmental Hazards on the Machine Frame

Once connections are moved out of the cabinet, severe vibration from motors and automated guided vehicles threatens to loosen threaded connections over time. Beyond vibration, exposed connections face physical threats from moisture ingress and exposure to industrial lubricants during normal operation or industrial cleaning agents during high-pressure washdowns.

Electrical noise is another major concern. Variable frequency drives generate significant EMI that threatens nearby digital signals. Shielded cables remain the industry standard for protecting machine-mounted data runs against this interference. However, operators must properly ground these shields to prevent ground loops that amplify EMI across the factory floor. Alternatively, facilities manage interference by maintaining strict physical separation between unshielded Ethernet cables and power lines.

Modular Hardware Solutions for On-Machine Distributed I/O and Fieldbus Networks

Adopting on-machine distributed I/O directly solves the physical and logistical obstacles of traditional wiring. Implementing machine-mounted distribution, along with hybrid interfaces and quick-locking connectivity, helps engineers accelerate commissioning while protecting signal integrity in harsh environments.

Machine-Mounted Distribution

Integrating machine-mounted IO-Link masters directly on the equipment bridges the gap between discrete sensor signals and higher-level industrial Ethernet networks. At the same time, placing IP65 and IP69K-rated devices directly on the equipment removes the need for bulky protective enclosures. This plug-and-play connectivity allows integrators to build and test systems on the shop floor before simply unplugging the cables for shipment. Reconnecting devices and machinery using pre-tested cables at the end-user facility drastically cuts installation time and reduces the risk of manual wiring errors.

Ruggedized Environmental Protection

To survive outside the cabinet, selecting the right cable jacket material protects the connection from specific environmental hazards. While PVC suits less -demanding applications, upgrading to appropriately rated PUR or TPE jackets protects the connection against UV exposure, harsh industrial lubricants, cleaning agents and premature mechanical failure in continuous flexing applications. Beyond the cables themselves, advanced connector sealing and coupling options protect sensitive contacts from moisture and high-pressure washdown conditions.

Hybrid Interfaces for Power and Data

While some facilities prefer separate cables to isolate troubleshooting efforts, hybrid interfaces combine power and data in a single cable to save valuable real estate on the machine frame. For example, motor controllers benefit from combining high voltage with temperature sensing and brake controls in one streamlined cable. Combining power and Ethernet continues to gain popularity in modern automation systems. Engineers reduce overall cable counts by delivering operating voltage directly through the network connection using Power over Ethernet (PoE) or Power over Data Line (PoDL) technology. For more demanding applications, hybrid M12 connector systems like Molex Circular Hybrid Technology provide a dedicated physical interface to route both power and high-speed data simultaneously.

Quick-Locking Technology

To speed up installation, push-to-lock mechanisms, commonly referred to as “push-pull” technology, replace traditional threaded nuts to accelerate field preparation. Eliminating manual torquing saves significant time and prevents ergonomic strain on assembly workers' fingers. Once installed, the locking design intrinsically resists heavy vibration, keeping connections secure during continuous operation. Ultimately, establishing a reliable physical layer gives facilities the stability needed to support advanced data processing and future automation trends.

High-Bandwidth On-Machine Connectivity for Edge AI and Advanced Robotics

As industrial robotics evolves, the industry continues to expand the physical limits of hardware to support artificial intelligence. Integrating AI directly at the device level forces engineers to rethink how they route power and data across the factory floor.

Looking ahead, machines could soon be asked to process and transfer exponential amounts of data between humanoid cells and modular systems. To achieve this, decentralized devices would need to communicate directly with a central AI hive to optimize the entire manufacturing process. Supporting these high-speed networks requires advanced physical hardware capable of handling increased bandwidth while consuming more power. Technologies like Single-Pair Ethernet (SPE) are set to handle this massive influx of data once device manufacturers fully adopt the standard. Preparing for this next generation of automation means selecting rugged interconnect solutions that fit into increasingly tight spatial footprints.

Molex Ruggedized Interconnects for On-Machine Infrastructure

A complete hardware portfolio, backed by deep engineering support, helps customers develop a connectivity architecture tailored to their specific application. Molex provides the rugged connectivity and design expertise needed to deliver power and data from the control cabinet directly to the machine frame.

To combat severe vibration and reduce field preparation time, Brad M12 Ultra-Lock 2.0 cable assemblies provide an IP69K seal and a push-to-lock mechanism that cuts installation time by up to 70 percent compared to standard threaded options. Additionally, to save valuable real estate without sacrificing power, Brad M12 Power L-Code connectors and cable assemblies deliver up to 16.0A in a compact 12.00mm footprint, replacing much larger legacy 7/8” mini-change connectors. To prepare factory floors for future high-speed data needs, Industrial Single-Pair Ethernet connectors and cable assemblies connect sensors directly to the Ethernet ecosystem.

The Molex engineering team goes beyond standard commodity cables to develop custom solutions for highly specific industrial applications. Having pioneered modular plug-and-play industrial wiring and connectivity solutions, Molex brings decades of field-level application experience to help customers build reliable on-machine distributed I/O networks today.

Discover how Molex industrial automation connectors can help you reduce cabinet volume and protect signal integrity in your next decentralized design.

Additional Resources


Application

Next-Generation Industrial Automation Connectors

Centralized hardwiring adds complexity to machine builds, monopolizes valuable floor space and increases the risk of installation errors and commissioning bottlenecks. See how modular, plug-and-play decentralized connectivity can simplify installation, withstand harsh environments and future-proof the factory floor for Edge AI and robotics.

Robotic arms assembling products on a factory production line utilizing advanced industrial automation connectors.

Share