Read Time: 4 Min
As the industry races to support next-generation AI accelerators and GPUs, data centers face unprecedented power demands. Racks that historically drew 20 to 30kW of power now scale to 120kW, 150kW and even approach 1MW. At these extreme levels, traditional air cooling simply cannot provide sufficient heat transfer.
While direct-to-chip liquid cooling has become standard for compute components, power distribution has struggled to keep up. The power delivery path itself has become a critical thermal bottleneck in the modern rack. Adapting to advancing processors means rewriting the rules of rack design and cooling the power delivery path from the inside out.
The Breaking Point of Air-Cooled Power Distribution
While air-cooled busbars remain a reliable and cost-effective solution for lower-power applications, conventional power-routing methods face hard physical and thermal limits as rack-level current requirements continue to rise. Standard air-cooled busbars and the heavy cabling needed to connect them simply take up too much rack space and generate excessive heat. Moving from these thick, insulated cables to a rigid busbar system reclaims valuable real estate and often achieves a 3-to-1 or 4-to-1 size reduction.
However, rising current loads require thicker, heavier copper busbars, which ultimately block the airflow needed to cool the servers. This physical crowding limits design options and fails to provide compute components with sufficient cooling. As power loads approach 150 to 160kW (roughly 3,000.0A), the physics of air cooling break down, resulting in a temperature rise (ΔT) that exceeds standard operational limits.
When traditional busbars trap excess heat, they create localized hot spots that threaten the rack’s overall thermal stability. Elevated conductor temperatures increase electrical resistance, causing severe voltage drops and significant energy waste. The resulting cycle limits overall system performance and exerts long-term mechanical stress on connections due to constant thermal cycling.
Integrating Liquid Cooling for Server Rack Power and Thermal Management
Liquid-cooled busbars merge server rack power and thermal management into a single, unified system. By combining an optimized conductor design with integrated cooling channels, this architecture creates a robust platform for distributing extreme currents in space-constrained environments. Instead of relying on external airflow to cool the power distribution hardware, liquid-cooled busbars mitigate heat directly at the source.
Eliminating Thermal Derating with Liquid Busbar Cooling
Locking in a low and stable temperature fundamentally changes the math for electrical design engineers. In legacy setups, engineers must calculate for thermal derating, knowing the busbar will carry less current as it heats up. Liquid busbar cooling prevents heavy power losses typically caused by overheated copper. This approach provides dependable, efficient electrical performance, allowing systems to push higher currents without the penalty of increased resistance.
Mitigating Risks with Copper-to-Copper Welding
Bringing liquid near high current introduces inherent risks, such as leaks, condensation and potential short circuits. Advanced liquid-cooled busbars address these valid engineering concerns through strict manufacturing and testing protocols.
Instead of relying on mechanical seals or O-rings, the most reliable designs use copper-to-copper welding. Since both parts are made of the same material, their uniform thermal expansion prevents the cracks and leak paths that are common when dissimilar materials heat and cool at different rates. To validate this structural integrity, rigorous pressure and leak testing must be performed on these components before deployment.
Maintaining Standard Mechanical Footprints
Even with fluid channels, liquid-cooled busbars match the standard high-power rack (HPR) and ORv3 mechanical footprints for easy swapping. Since the mounting interface remains identical to air-cooled versions, data centers can scale power loads and transition to liquid busbar cooling without expanding the busbar’s physical footprint or forcing rack infrastructure trade-offs.
Preparing for Evolving Rack Standards
The rapid evolution of AI technology is prompting industry standards and data centers to live in a state of ongoing revision. Preparing for tomorrow’s processors calls for a clear view of where server rack power architecture is headed.
The Role of OCP and Shared Specifications
Standards organizations like the Open Compute Project (OCP) continuously evolve as rack power thresholds climb. While full-rack immersion cooling generated significant research interest in recent years, much of the industry's immediate attention has shifted toward targeted liquid-cooling solutions. Future OCP iterations will likely establish formal guidelines for liquid-cooled power distribution.
Upgrading Infrastructure for 1MW Racks
Leading hyperscalers are already planning design iterations that push the limits of power density, including conceptual work on 1MW IT racks. Supporting this magnitude of power would compel data centers to overhaul their core infrastructure, integrating coolant distribution units (CDUs) and routing liquid manifolds directly to the rack level.
Supporting a Phased Transition
Scaling data center racks from 20kW to 1MW requires significant infrastructure changes that cannot be implemented overnight, spurring demand for flexible solutions to support a phased transition. For example, a facility might install a liquid-capable busbar today and operate it safely within an air-cooled architecture until the broader liquid-cooling architecture is fully deployed. This flexibility offers a practical path forward, protecting investments in existing platforms while preparing for future demands.
Active participation in OCP working groups allows component manufacturers to help shape these emerging standards. Molex engineers collaborate directly with industry leaders to confidently align new liquid-cooled busbar designs with future specifications, so customers are prepared for the next wave of power density growth.
Advanced Liquid Busbar Cooling: The Molex Multi-Channel Solution
While liquid-cooled busbars have become mandatory for high-density racks, the internal geometry of the coolant pathway determines the ultimate efficiency of the system. Molex engineers have unlocked a proprietary leap by moving beyond standard single-channel designs.
Optimized Multi-Channel Geometry
Unlike single-channel aluminum tubes, which are prone to corrosion, Molex Multi-Channel Liquid Cooled Busbars use extruded copper tubes segmented into up to three discrete channels. This layout increases contact surface area and creates optimal turbulent flow, yielding greater cooling efficiency than single-channel alternatives. It delivers this superior performance in half the physical space (25mm² versus 50mm²), leaving more room for critical compute hardware.
Future-Proof Performance and Integration
Setting a major benchmark for thermal efficiency, the busbars maintain a ~30CΔT at 15,000.0A. A strategic design roadmap to 25,000.0A eliminates costly rip-and-replace redesigns and protects investments in existing platforms as AI power loads grow.
The liquid-cooled solution minimizes pumping power with a wide flow range (1 to 10 liters per minute) and a sub-1-bar pressure drop at 2 LPM while supporting both dielectric and non-dielectric liquids. A plug-and-play interface with configurable dimensions and fluid connection points accommodates tight layouts. Each busbar undergoes a 100% line inspection, including rigorous helium and pressure leak testing, before it leaves the facility.
By unifying server rack power and thermal management into a single component, Molex provides a practical path forward for scaling next-generation AI infrastructure. Explore Molex Multi-Channel Liquid Cooled Busbars to scale power without sacrificing valuable rack space.
Additional Resources
Share