Apr 23, 2018
Lisle, IL and Fridolfing, Germany – April 23, 2018 – Molex and Rosenberger have signed a dual-sourcing agreement allowing Molex to produce High-Speed FAKRA-Mini automotive coaxial connectors based on the Rosenberger HFM® design. Enabling fast transmission of high data rates up to 20 Gbps, the Rosenberger HFM FAKRA-Mini system is designed for a range of existing and future automotive applications, such as advanced driver assistance systems (ADAS), navigation, infotainment and intelligent connected vehicles.
With the dual sourcing agreement, Rosenberger and Molex provide a high-quality, high-speed, cost-optimized intermateable interface with identical mechanical and electrical performance and features. The solution delivers seamless backward compatibility for the automotive market.
“Molex is excited to collaborate with Rosenberger to launch the dual-sourced HFM solution that enables high-speed data transmission fundamental to connected vehicle technology,” said Ryan Price, networking segment director, Molex. “Our shared vision is to deliver a high value, cost effective solution that provides design flexibility and backward compatibility.”
With the increasing bandwidth and safety critical needs of connected and autonomous vehicle architectures, it is necessary to have a robust infrastructure that can operate a multitude of devices, screens and cameras. HFM FAKRA-Mini connectors allow for the highest bit rate data transmission while saving up to 80 percent of installation space and significant weight compared to the conventional FAKRA generation.
“Ensuring safety is the ultimate priority of ADAS and autonomous driving systems, and HFM connectors play a key role in processing the high data volumes from cameras, sensors, navigation sources and other external objects in real time,” said Dr. Tosja Zywietz, CEO, Rosenberger. “We are pleased to collaborate with Molex on making this next-generation coax connector widely available to the automotive industry as a quasi standard."
There is no investment relationship between Molex and Rosenberger under the terms of the product dual-sourcing agreement.
About Rosenberger:
Rosenberger Hochfrequenztechnik GmbH & Co. KG was founded in 1958. A family owned company, Rosenberger ranks today among the world-wide leading manufacturers of standard and customer-specific connectivity solutions in high frequency, high voltage and fibre optic technology. The product range covers RF coaxial connectors, RF test & measurement products, RF connectors for automotive electronics, medical and industrial electronics as well as fibre optic products, and cable assemblies. Renowned companies in high-tech industries, e.g. telecommunication, data systems, medical electronics, industrial electronics, test & measurement, aerospace engineering or automotive electronics trust the precision and quality of Rosenberger products. Rosenberger is certified to IATF 16949, DIN EN 9100, ISO 9001 and ISO 14001.