Ventilators are critical in the global response to the new coronavirus but use of these devices requires significant training from specialized healthcare providers. The SAVe II ventilator from AutoMedx, a Molex customer, overcomes this training hurdle by simplifying use without sacrificing effectiveness.
It is extremely portable, weighting just 2.7 lbs. with up to 10 hours of battery life on a single charge, and nurses and doctors can be trained to use the SAVe II in only 1-2 hours. A body height selector on the device corresponds to preset tidal volumes — the volume of air normally displaced by the lungs without applying extra effort — to reduce error and give healthcare professionals time to care for other patients. This ventilator was originally developed to improve triage capabilities on the battlefield where weight and ease-of-use are crucial, but its simple operation and reliability make it an appealing option for healthcare providers without formal ventilator training to effectively treat patients with COVID-19.
However, the pandemic increased demand for the SAVe II by approximately 25x, meaning Molex, as the supplier of multiple critical components, also needed to quickly increase production.