Skip to main content
Construction Worker

Revolutionary RFID Solutions Catering to Smart Factory, Logistics and Medical Applications

RFID technology offers cost-effective solutions to a range of challenges. Innovative RFID tags with embedded chips and sensors can improve supply chain performance, asset management and factory efficiency.

By: Bob Mahre
Business Development Manager

Read Time: 5 Min

Kinesthesia is sometimes called the sixth sense. It is the ability to sense where the body is and what it is doing – for example, not having to look at one’s arm to know it is outstretched. This level of awareness is a crucial capability, and not just for people. Think about a factory or manufacturing setting: knowing what the different parts of the system are doing and how they’re functioning at all times is critical to efficiency. The same is true of the supply chain. For manufacturers, distributors and logistics providers, knowing the location and condition of individual products and shipments is vital.

The key to this level of awareness is connectivity, and the key to connectivity today is radio frequency (RF) wireless communication. Radio frequency identification (RFID) has been used for years in asset tracking and inventory control, but recent advancements in the capabilities of RFID tags – and the hardware and software used to communicate with them – have introduced exciting new possibilities.

RFID Tag Capabilities

RFID tags are useful for a wide range of applications and are available in many different forms to meet varied demands. Traditional hard tags, flexible tags, cable tie tags, adhesive labels, ferrite tags and molded PCB tags can all be leveraged in industries spanning medical to industrial to supply chain and many more. Tags are available for both high-frequency (HF) and ultra-high frequency (UHF) applications, with UHF tags offering a far greater read range so that operators can read the tag from dockside or across a warehouse. Customization is also possible — certain tag designs include a built-in antenna, LED and chip.

Incorporating a chip into the RFID tag opens a host of additional capabilities. Depending on the chip, the RFID tag can become a sensor, enabling the tag to sense temperature or humidity and then log and store that information. A battery-powered RFID tag can create a record of its environment over time that can be retrieved and analyzed. 

RFID tags are helpful for authenticating products to mitigate the risk of mistakes. For example, in the medical field, a device can be programmed to operate exclusively with specifically tagged cartridges and sensors, thereby minimizing the potential for unintended errors and preventing the utilization of counterfeit products.

RFID tags fitted with LEDs can also act as real-time warning devices. They can be set to activate after a certain period or to alert users of environmental conditions outside of given parameters. This information can be retrieved with a handheld or mounted RFID reader or even a smartphone. By reducing the requirement for specialized hardware, RFID tags are accessible to more users. 

Smart Factory Applications

Wireless communication is critical to effective performance in the smart factory of Industry 4.0. RFID tags have long been popular for inventory control and tracking. With innovations such as low-profile RFID labels and new developments in miniaturized RFID solutions, it is possible to track products in inventory and throughout the manufacturing process. By creating a fully formed picture of how the entire factory is functioning, significant potential exists for process improvement. Robust RFID capability and targeted analytics can help manufacturers identify bottlenecks and methods to accelerate the process – thereby saving time and money.

Logistics Applications

The sensing capability of RFID tags is especially valuable in logistics and shipping. Many products, particularly in the food and beverage and medical industries, must be kept within a specific temperature or humidity range throughout the shipping process. An RFID tag with a chip capable of sensing these environmental conditions can record the parameters at preset intervals. Upon arrival at the destination, this information is easy to read and can confirm that the product has been stored according to requirements. This ability to confirm safe storage conditions throughout the shipping process can help prevent a range of issues with spoiled or unusable products.

Medical Applications

Factory Worker

The advantages of integrating RFID communication into the product life cycle are clear in the medical and pharmaceutical industry. RFID tags with chips can be added to individual products to fulfill several purposes. In addition to inventory tracking and verification, RFID tags can track temperature and humidity to warn of potential problems. Manufacturers can also preprogram RFID tags equipped with LEDs for a set period. The LED can light up when the product is expired or to enhance inventory management. For example, the LED can illuminate when the product is getting near the end of its shelf life so that users know to use a particular item before it expires. This capability can offer enormous savings in addressing the problem of inventory loss due to expiration.

RFID tags are also a method of ensuring proper authentication for medical products that require use with a specific type of equipment or medicine. The tag can incorporate a chip that detects whether the product is being used properly. Approved equipment or medication with an RFID tag permits the tag to authenticate. This can help prevent the use of improper or even counterfeit products, including unauthorized equipment or incompatible drugs.

Customized Solutions

With a global manufacturing base and decades of experience, Molex offers robust support for customers in many industries, including manufacturing, logistics and medical. Molex carries 17 distinct types of RFID tags in various frequency bands and with different designs and attachment methods depending on the application. Using a standard Molex RFID product ensures rapid deployment, sourcing flexibility, lower cost and simplified development.

Molex also offers a convenient solution for downloading data from RFID tags, providing two options for seamless access. Users can utilize either a handheld RFID reader or their own smartphone equipped with Molex's dedicated app, available for download for both iOS and Android devices. This versatile approach ensures that users can effortlessly receive and download data from RFID tags, catering to their specific preferences and devices.

Where Molex truly stands apart is with customized connectivity solutions. Molex provides numerous advantages for companies seeking RFID solutions tailored to specific needs:

  • Robust cross-discipline engineering support throughout the design process
  • Extensive collaboration and customization ability
  • Global manufacturing footprint
  • Decades of experience in RF technology

Custom RFID solutions can include built-in chips, battery power, LED notification and other capabilities in several tag types. Molex RFID solutions can address a host of needs for smart factory, logistics or medical applications. Get more information on finding the right solution to address various challenges when you start the conversation with Molex.

 

 

 

Share

   

Related Products


RFID Products

Printed Circuit Solutions

Related Industries