You may have already read about my 50:50:50 rule when it comes to the choice using tin plated surfaces versus gold plated surfaces in connectors. This rule says tin is the more economical solution if you have less than 50 contacts (mating forces), if you can live with 50 mating cycles (contact normal forces), and if you do not expect less than 50 milliohms contact resistance over life time. The higher contact normal forces for tin plated surfaces (>2 Newton end of life) result in higher mating forces which limit the amount of contacts in a given connector and the un-noble tin does have a higher contact resistance, compared to gold or nickel palladium.
Besides these basic rules there are some other limitations where gold (or palladium nickel) must be used:
- For any type of analogue signals, gold is a must because of line noise created by tin plated contacts
- For any connector being exposed un-mated in the field in an industrial atmosphere
- For any connector with a contact spacing of less than 1mm because of whisker growth of pure tin-plated non annealed surfaces
Especially the 3rd item created a lot of confusion in the industry when lead-free tin surfaces were introduced years ago. FFC connectors do have contact spacing below 1mm and the connector industry strongly recommended the use of gold-plated FFC connectors which connect either FPCs or FFCs, however, the cable industry was not yet able to supply gold plated FFC cables. So some designers were forced to mate gold-plated FFC connectors with tin-plated FFC cables, a mortal sin when it comes to reliability!
Gold and tin in one mated connector system is a no go. The behavior of these two platings is not well researched, however, the standard electrode potentials tell you that the contact point will corrode (gold = +1,5V tin = +0,15V – look at your rainwater gutter when copper meets zinc) and the reliability is gone.
Years ago, I asked Molex’s contact physics guru about this subject in a special case and this was his in-depth answer: