Skip to main content
Image

Wearable Healthcare Technology

The shift toward human-centered healthcare and remote patient monitoring has prompted the rise of new medical devices worn by the user. These compact innovations combine advanced capabilities with unprecedented ease of use, enabling real-time tracking that can help optimize treatment. As their potential continues to grow, Molex supports customers with globally integrated capabilities and specialized solutions that help maximize market success.

Overview


The latest developments in miniaturized electronics and high-speed wireless connectivity have created a promising range of new product opportunities. As the healthcare industry embraces the value of remote patient monitoring and human-centered care, for example, studies indicate that a rapidly growing number of individuals utilize some type of connected medical wearable device to facilitate tracking and/or treatment from home or virtually any location. 

Medical wearables like continuous glucose monitors (CGMs) often appear simple on the outside to help support ease-of-use across patient populations. However, those straightforward exteriors reflect a complex array of interrelated engineering choices behind the scenes. Product innovations that achieve widespread industry adoption typically embody a careful balance of key characteristics like durability, usability, biocompatibility and standards compliance. Today’s manufacturers need to pack intelligent capabilities into increasingly compact form factors while remaining mindful of ingress prevention, industry certification, supply chain sourcing, strategic design-for-assembly and more. At the same time, they’re attempting to integrate a complicated assortment of data and digital technologies while remaining mindful of sustainability, supply chain hurdles and shifting regulatory standards.

It’s an increasingly precarious journey from early prototype to full-scale product realization — which is why today’s forward-thinking organizations often enlist the specialized assistance of skilled design and manufacturing providers like Phillips-Medisize, a Molex company. As an end-to-end, globally integrated product realization resource with robust proficiency across highly regulated industries, Phillips-Medisize helps customers bring innovative medical wearables to life with expertise that includes high-performance medical interconnects, microelectronics, complex custom cable assemblies, ISO 13485 quality management, precision injection molding and more.  


Continuous Glucose Monitoring (CGM) Devices

To make more effective devices, CGM designers must address user experience requirements, strict regulatory constraints, compact space limits and power distribution, among other concerns. Find out how Molex experts are helping manufacturers manage the complexities of CGMs and other medical wearables.

Wearable Insulin Pumps

The design of insulin pumps must balance patient safety, accurate dosage delivery and usability inside a highly compact design footprint. See how Molex experts leverage advanced technology solutions and customized capabilities for advanced wearable insulin delivery.


Blog

Overcoming Medical Wearable Design Integration Challenges

Miniaturizing medical wearables requires a careful balance between comfort, reliability and performance in a much tighter space. Learn how a system-level approach helps engineers manage these design trade-offs.

An adult uses a smartphone to monitor data from a compact medical wearable sensor on their upper arm.

Blog

The Consumerization of Healthcare: A New Landscape for Medical Device Design 

How are medical wearable designers keeping pace with user demands while navigating strict regulations?  

Designing Wearable Medical Technology

What does it take to design the latest wearable devices? Read how Molex has accepted the challenge.

Image

Flexible Circuits for Medical Wearables

Flexible printed circuits offer significant advantages over traditional, rigid printed circuit boards. Read how Molex flexible circuits are helping the designers of future medical devices.

Image

CASE STUDY

Phillips-Medisize Helps GlucoModicum Develop Needle-Free Wearable Innovation

Unified collaboration addressed human-centered design, risk management and commercialization challenges to create a proprietary, non-invasive continuous glucose monitor (CGM).