March 12, 2024 (Originally published on AirBorn.com)
GEORGETOWN, Texas, March 12, 2024 – AirBorn, a leader in designing, qualifying, and manufacturing rugged electronics is proud to announce the release of their new VPX power supply. With a maximum output power greater than 2300 watts, the series sets a new standard for VPX power density and efficiency.
The power system is a 6U power supply that offers the highest overall VPX power density and power efficiency available today. It meets the VPX and VITA 62 open architecture and performance requirements. Notably, it delivers nearly twice the output of traditional 6U power supplies with a remarkable efficiency of 95%. This allows customers to support the higher power levels required in modern defense applications without increasing the size of their power supply units.
"New defense electronics solutions often have higher power consumption. Our new VPX power supplies can satisfy both the SWAP-C requirement and the need for state-of-art performance," said Michael Blanchfield, AirBorn Product Group Director.
In addition, the VPX system meets MIL-STD-461 conducted EMI emission requirements without external filtering. “This unique feature offers cost and space savings compared to alternative solutions on the market,” explained Scott Poole, Director of Engineering for AirBorn’s Power Group.
The VPX power supply is an intelligent power solution that meets and exceeds the evolving needs of modern defense applications. The embedded intelligence allows flexible sharing through dispatchable power which can be configured to control voltage, balance current or temperature across multiple power supplies. Additionally, the power system's intelligence allows system designers to utilize a dual data bus communication where a system controller or chassis manager can talk to the power supply and inquire about input voltages, output cards, power temperatures, and other information from the power supply, possibly predicting failures.
With over 30 years of experience in power supply design and manufacturing, AirBorn's VPX power supply is an embodiment of the company's technical expertise, commitment to quality, and dedication to customer satisfaction. It is not just a power supply; it is an intelligent power solution that meets and exceeds the evolving needs of modern defense applications.
For more information about the VPX Power Supply or any other AirBorn products, visit www.airborn.com.