Tracing who has a virus is an important step in containing its spread —especially in public spaces or dense, urban areas. And with the challenging dynamics of the COVID-19 pandemic – it has never been more vital. Thermal imaging scanning identifies the heat generated by fever, a common symptom of COVID-19. With expertise and support from Molex, one global leader in thermal imaging cameras was able to address an unexpected spike in demand for this critical technology.
The company’s advanced cameras offer a non-invasive, safe and anonymous way of thermally scanning people in heavily populated areas such as airports or train stations. Their cameras look at specific zones on the body, such as the forehead or the corners of the eyes, to detect a potential fever.
However, a camera is only as effective as its user interface.
Molex’s design, components and development expertise ensured that the cameras are easy-to-use, while controlling for higher costs and production times.