| Good Crimps and How to Recognize Them | ![]() |

You've made it through all the connector catalogs, found the connector that meets all your design criteria and is just right
for your application. With the right current rating, voltage
rating, circuit size, engagement force, wire AWG capabilities,
configurations, termination method and safety features, e.g.
positive locks, fully-isolated contacts, polarization and agency
certifications, it is, in short, the perfect connector.
But don't let out a huge sigh of relief quite yet --especially
if the connector you've chosen uses a crimp termination system.
While this can be one of the fastest, most reliable and rugged
termination methods, if the terminal isn't crimped onto the wire
correctly you can forget all about the hard work you put into
selecting the right connector. And, although there are 13 common
crimping problems that can reduce the reliability of your
product, these problems are easy for you to avoid with a little
knowledge and advance planning.
To begin with, it helps to understand that a terminal has three
major sections: Mating, Transition and Crimping (Illustration
A). The Mating section, as the name implies, is the section of
the terminal that mates, or becomes the interface, with the
other half of the connection. This section was designed to mate
with a terminal of the opposite gender and to perform in a
certain manner by the connector design engineer. Anything that
you do that deforms the Mating Section, especially during the
crimping process, will only reduce the connector's performance.
The Transition Section also is designed so that it would not be
affected by the crimping process. Here again, anything you do
that changes the position of the Locking Tangs or Terminal Stop
affects the connector's performance.
The Crimp Section is the only section that the crimping process
is designed to affect. Using termination equipment recommended
by the connector manufacturer, the crimp section is deformed so
it can be securely attached to a wire. Ideally, all the work
that you do to crimp a terminal onto a wire occurs only in the
Crimp Section.
An example of a properly performed crimp is seen in Illustration
B. Here, the insulation crimp compresses the insulation without
piercing. The wire strands (or brush) protrude through
the front of the conductor crimp section by at least the
diameter of the wire's conductor. For example, an 18 AWG wire
would protrude at least .040". Both the insulation and conductor
are visible in the area between the insulation and the conductor
Crimp Section. The conductor Crimp Section shows a bellmouth
shape in the leading and trailing ends, while the Transition and
Mating Sections remain exactly the same as they were before the
crimping process.
If your crimped terminal does not look like the terminal in
Illustration B - the problem may have been caused by something
that went wrong during the crimping process. Here are 13 of the
most common problems that may occur during the crimping process
and what you can do to avoid them.


The crimp height, which is the cross sectional height of the
conductor Crimp Section after it has been crimped, is the most
important characteristic of a good crimp. The connector
manufacturer provides the crimp height for each wire size for
which the terminal was designed. The correct crimp height range
or tolerance for a given wire may be as small as 0.002". With a
specification this tight, verifying that the press is setup
correctly is very important for achieving a good crimp.
A crimp height that is either too small (Figure I) or too large
(Figure II) will not provide the specified crimp strength
(terminal retention to the wire), will reduce the wire pull out
force and current rating, and may generally cause the crimp to under
perform in otherwise normal operating conditions. A crimp height
that is too small also may cut strands of the wire or fracture
the metal of the conductor crimp section.


A crimp height that is too large will not compress the wire
strands properly, causing excessive voids in the Crimp Section
because there is not enough metal-to-metal contact between the
wire strands and the metal of the terminal.
The solution to problems #1 & #2 is very simple: adjust the
conductor crimp height on the crimp press. Using a caliper or micrometer as shown in
Illustration B, verify that the crimp height is within
specification when the press is first used for a production run
and recheck it as frequently as necessary during the run to
maintain the proper crimp height.


Connector manufacturers do not typically supply a crimp height
for the insulation due to the variety of insulation types and
thicknesses. The insulation crimp provides a strain relief for
the conductor Crimp Section so that as the wire flexes, the wire
strands do not break. An insulation crimp section that is too
small may overstress the metal in the insulation Crimp Section,
weakening the strain relief function.
Most types of crimp tooling allow the insulation crimp height to
be adjusted independently of the conductor crimp height. The correct adjustment allows
the terminal to grip the insulation for at least 180 degrees
without piercing the insulation. An insulation displacement, or
compression where the OD of the terminal's insulation crimp and
the OD of the insulation are approximately the same, is ideal.
5. Loose Wire Strands
Loose wire strands (Figure V) are another common cause of crimping problems. If all
the wire strands are not fully enclosed in the conductor Crimp
Section, both the strength of the
crimp and the current carrying capability may be greatly
reduced. To get a good crimp you need to meet the crimp height
the connector manufacturer specifies. If all the strands are not
contributing to that crimp height and therefore, crimp strength,
then the crimp will not perform to specifications. Generally,
the problem of loose wire strands is very easy to solve by
simply gathering the wires back into a bunch before inserting
them into the terminal to be crimped. The strands may have been
inadvertently separated during the handling or bundling process
if stripping the insulation from the wire is done as a separate
operation. Using a "strip and retain" process for insulaton
removal, where the insulation slug is not completely removed
from the wire until it is ready to have a terminal crimped onto
the wire, helps minimize the problem.

If the strip length is too short or if a wire is not fully
inserted into the conductor Crimp Section, the termination may
not meet the specified pull force because the metal-to-metal
contact between the wire and the terminal is reduced. As shown
in Figure VI, the strip length of the wire is too short (note
that the insulation is in its proper position), not allowing the
required one wire OD extension in front of the conductor Crimp
Section. The solution is simple: increase the strip length of
the wire stripping equipment to that specified for that specific
terminal.
7. Wire Inserted Too Far
Another crimping problem that relates to a too short strip
length occurs when the wire is inserted too far into the crimp
sections. As Figure VII shows, the insulation is too far forward
of the insulation Crimp Section and the conductors protrude into
the Transition Section. This may cause as many as three failure
modes in the actual application. Two relate to a reduced current
rating/wire pull out force due to a reduction of the metal-to-
metal contact in the conductor Crimp Section. A metal-to-plastic
contact isn't as strong, nor does it conduct electricity, as
well as metal-to-metal.
The third failure mode may occur when the
connectors are mated. If the wire protrudes so far into the
Transition Section that the tip of the male terminal hits
against the wire, it may prevent the connectors from fully
seating or it may bend the male or female terminals. This
condition is known as "terminal butting".
Under extreme cases, the terminal may be pushed
out the back of the housing even though
it was fully seated in the housing. To solve this problem, make
certain the wire is not inserted into the press with so much
force that it overcomes the wire stop on the press, or adjust
the position of the wire stop so that it correctly axially
positions the stripped wire.
8. "Banana" (Excessive Bending) Terminal
One of the most descriptive crimping problems is known as a
"banana" crimp (Figure VIII), because the crimped terminal takes
on a banana shape. This makes it difficult to insert the
terminal into the housing and may cause terminal butting. This
problem is easy to solve by adjusting the position of the hold
down pin on the crimp press. This small pin is located in the
crimp press and contacts the terminal in the mating section
while the crimp sections are being crimped onto the wire. During
crimping, a significant amount of metal on one end of the
terminal (in the crimp section) moves. These high forces tend to
force the front of the terminal upwards, unless it is held down
by the aptly-named "holddown pin".
One of the more obvious crimping problems is when part of the
Transition Section is
damaged, as shown in Figure IX. In the terminal shown, the tab
sticking up is a design feature called a "terminal stop". Its
function is to prevent the terminal from being inserted too
deeply into the housing. If the stop is extremely damaged, the
terminal can actually be pushed all the way through the housing.
The solution is relatively simple. What causes the problem is
that the terminal and carrier strip (the band or strip of metal
the terminals are attached to when you receive them from the
manufacturer) is not properly located with respect to the press.
To solve it, simply loosen the base plate of the interchangeable
tooling and realign it to the press.
The correct size for a bellmouth (Figure X) is approximately 2X
the thickness of the terminal material. For example if the
terminal is made from material that is .008" thick, the
bellmouth should be approximately .016". While a few thousands
of an inch either way will not materially affect the terminal's
performance, if the bellmouth is missing or if it is less than
one material thickness, there is a risk of cutting the wire
strands. The fewer strands that remain, the lower the
termination strength. To correct the problem, make sure the
punch and anvil on the crimping equipment are properly aligned.
There is also a problem if the bellmouth is oversized (Figure
Xl), because this reduces the total area that the crimp section
of the terminal has in contact with the wire. The less the
wire-to-terminal interface, the lower the wire pull out force.
If the crimp height is correct, then it is likely the problem is
caused by worn tooling, which should be replaced.
The carrier strip is cut off of the terminal during the crimping
process. If the remaining cutoff is too long (Figure XII),
problems can occur. The extra metal may protrude out the rear of
the connector when the terminal is inserted into the housing,
causing the connector to arc between adjacent contacts when
higher voltages are applied. If the carrier cutoff at the front
of the terminal is too long, the extra length may interfere with
connector mating and result in "terminal butting".
The solution is fairly simple. Adjust the baseplate on the press
so the terminal is centered properly in the crimp press.
Another indication that the terminal is not centered correctly
is that the bellmouth isn't properly former either. This
occours because the tooling for the bellmouth and the carrier
cutoff are spatially related.
Although bent lock tangs are not necessarily the result of a
poor crimping process, the connector can fail just the same.
Lock tangs (Figure XIII may be bent either in or out too far,
which impacts the terminal's ability to completely lock
into the shelf in the housing that was designed for this
purpose. The tangs may be damaged as the terminals are unwound
from the reel if the friction wheel on the reel holder of the
crimp press is too tight or it can be caused by handling after
the terminals are crimped onto the wires. Typically, terminated
wires are gathered into a bundle and inventoried or transported
to another location in the plant. During the bundling, or as
each terminated wire is removed from the bundle, the locking
tangs may be bent.
If the damage is occurring at the crimping
press, then the friction wheel needs to be adjusted so it is
only tight enough to keep the reel of terminals from being
unwound by their own weight. If the problem is occurring during the bundling
process, smaller bundles or improved handling procedures need to
be implemented.
While there are 13 problems that may be
caused during the crimping process, there are just four simple
rules that will help ensure a successful connector application:
1.Choose the right connector for your application requirements.2. Use the crimp tooling specified by the terminal manufacturer.
3. Properly adjust and maintain the crimp tooling in good working order.
4. Periodically replace the parts that displace metal (e.g. conductor and insulation punches, anvils and terminal cutters).
Since most of the problems that are reported to connector manufacturers relate to one of these thirteen crimping problems,
Molex offers an easy-to-use guide to help you avoid problems or
recognize them quickly enough so that you make only good crimps.
To order this guide contact Molex Incorporated, 2222 Wellington
Court, Lisle, Illinois 60532, Attention: Good Crimp Drawings.
*The parts of the crimp tooling that significantly displace the metal of the terminal - the conductor and insulation punch, anvils and the terminal cutoff tooling will need to be periodically replaced.